The Swagger specification of this service can be found here.
The Go client code for this service is available here.
The alarm status is, when calculated, sent as an event to an SNS topic. The format of the messages is documented here.
Various types used in requests and responses are represented by enumerations. Their meanings are documented below.
| Value | Type |
|---|---|
| 0 | NOT_CONFIGURED |
| 1 | NO_DATA |
| 2 | GOOD |
| 3 | ALERT |
| 4 | DANGER |
| Value | Type |
|---|---|
| 0 | NONE |
| 1 | OVERALL_IN_WINDOW |
| 2 | OVERALL_OUT_OF_WINDOW |
| 3 | INSPECTION |
| Value | Type |
|---|---|
| 0 | UNKNOWN |
| 1 | FIXED |
| 2 | SPEED_MULTIPLE |
Read more here.
| Value | Type |
|---|---|
| 0 | UNKNOWN |
| 1 | ABSOLUTE |
| 2 | RELATIVE_FULLSCALE |
| 3 | RELATIVE_OVERALL |
Read more here.
Information about the PAS API can be found here: